Tolerances for Mechanical Components: All You Need to Know

When designing mechanical parts, tolerances have a pivotal role. Here, we provide an overview of what mechanical components’ tolerances are and essential information for understanding them.

Discover more about Tolerances for Mechanical components

What are Tolerances for Mechanical Components?

Tolerance indicates the upper and lower limits of permissible values for errors that cannot be avoided during the manufacturing process.

 

For example, when attempting to machine a 50mm cylinder in processes like cutting, manufacturing precisely 50mm is impractical. Factors like material expansion due to temperature, machine expansion, and variations in material fixation, in fact, lead the machines in manufacturing with subtle errors. Therefore, while you can aim for “50mm,” achieving exactly 50mm is extremely challenging.

 

Hence, design and machining drawings specify the allowable error range as tolerance, which can be set for all the dimensions of a mechanical component.

Types of Tolerance

There are various types of indications for dimensions and shapes, and correspondingly, there are four types of tolerances:

General Tolerance

This is a tolerance applied collectively to individual dimensions. General tolerance, also known as standard tolerance, represents an allowable error range based on factors like machining methods and material size. In case of general tolerance, there are machining standards, so the designers can avoid setting specific value on their model.

Dimensional Tolerance

Dimensional tolerance pertains to the allowable error applied to specified dimensions in the drawing, including length, distance, position, angle, size, hole diameter, fillet radii, and chamfer dimensions. It is used when you want to specify tolerances different from general tolerance. In case of dimensional tolerance, designers have to specify clearly the tolerance value within the limits of the machining methods.

Geometric Tolerance

Geometric tolerance is used to define the range of errors that cannot be defined by dimensions alone. For instance, it’s employed when you need to specify the range of error for the position of two hole centers. It is specified on the drawing alongside dimensions.

Interference Tolerance

Interference tolerance refers to the accuracy of fits between shafts and holes. In this case tolerance has to be specified by the designers according to their plans.

The Relationship Between Tolerances and Manufacturing Costs

When assembling machine components, there are cases where a higher level of precision is required to ensure that the components fit smoothly. Such precision cannot be achieved with general tolerances. Therefore, it’s necessary to specify tolerances individually for dimensions.

 

When tolerances are specified, it’s essential to check if the post-machining dimensions fall within the specified tolerances. Furthermore, specifying higher-precision tolerances makes machining more challenging. In fact, to ensure to achieve the desired dimensions, more sophisticated machining tools will be deployed. Consequently, demanding higher precision in tolerances leads to increased costs in both machining and inspection. Therefore, when specifying tolerances, careful consideration is required to determine if the specified tolerance and precision are genuinely necessary.

Conclusion

Tolerances are defined limits for errors that cannot be avoided in the manufacturing process.

There are four types of tolerances: general tolerance, dimensional tolerance, geometric tolerance, and fit tolerance, which can be applied to different cases depending on the designers’ need.

 

Implementing tolerances might lead to an increase in costs. On the other hand, excessively loosening tolerances raises the risk of malfunctions. To balance product quality and costs, setting tolerances will lead to a perfect fit for your components while keeping the prices moderate.

 

By mastering tolerance design and calculations, you can achieve quality improvement while minimizing cost increases and cost reductions while maintaining product quality.

 

↑