Turning Parts Recognition Conditions

  • In the Machiend Plates, round shapes and edged shapes are automatically determined.
  • This section describes the recognition conditions.

Recognition of Turning parts

If the outer-most diameter has a cylindrical part, the shape is recognized for Turning Parts.
Recognition of Turning parts Recognition of Machined plates
  • 最外形が円筒部である
  • *The outer-most diameter is cylindrical
  • 最外形が四角である
  • *The external corner curved chamfer and outer-most shape form a rectangle
  • *The outer-most diameter cylindrical surface exceeds a total of 140°
  • 最外径が140°以下
  • *The outer-most diameter cylindrical surface is 140° or less

Outer- and Inner Diameter Recognition Conditions

The inner diameter and outer diameter are recognized based on their positional relationship with the central axis.
Recognition as “Outer- and Inner Diameter” Not recognition as “Outer- and Inner Diameter”
  • 自動見積対象形状
  • *Recognized as an “outer diameter” as it is on the central axis
  • 対象外形状
  • *Recognized as an “unsupported shape” not as an outer diameter, as it is not on the central axis
  • *Recognized as an “inner diameter” as it is on the central axis
  • 中心軸上にないため、内径ではなく「穴」として認識されます
  • *Recognized as a “hole” rather than as an inner diameter, as it is not on the central axis

Caution

  • Automatic recognition is not supported for external threads (outer diameter)
  • If a “internal threads (inner diameter) and hole” is recognized, the color attribute/CAD attribute link age function is enabled.>Automatic Hole Type Recognition

Keyway Recognition Conditions

  • For keyways that match the JIS (B 1301:1996), tolerances are automatically set and can be changed in the dialog. *The default settings can be customised in user settings.
  • *The default settings can be customised in user settings.

Caution

  • “If the inside corners are not rounded, the shape will not be recognised as an “outside groove” and the fit tolerance cannot be set.
  • If tolerance settings are required, design the groove with rounded corners that match the groove width.”

「外径キー溝・内径キー溝」の認識条件

以下の表に順次、規格内の場合認識されます。

注意

※2023年3月より対象となります。

b1/b2

2 3 4 5 6 8 10 12 14 16 18 20 22 25 28 32

焼き肌

Recognition Conditions of holes on the cylindrical surface

  • “A hole that is on the central axis is recognized as a “”hole”” supported for automatic quotation
  • If the hole does not turn on the central axis, it is recognized as an “”other hole”” and is not supported for automatic quotation.”
  • Even if no chamfer was modeled in 3D, a chamfer is produced at the hole entrance.
Recognized as a “hole” Not recognized as a “hole”
  • *Recognized as a “hole” as located on the central axis
  • *recognized as an “other hole” as not located on the central axis
  • Enter the hole information in the comments field to request a quotation

End Face Groove Recognition Conditions

If the bottom of the end face groove is curved it is not recognized. Design with sharp edges.
recognized as an “end face groove” Not recognized as an “end face groove”
  • *If the bottom has sharp edges
  • *If the bottom is curved