Add/delete angular dimensions and angular tolerances

Add angular dimensions and angular tolerances

1.Click Add Tolerance and click the two ‘surfaces’ to which you want to add dimensions.
2. Click where you want to display the dimensions.
  • The display position of the dimensions is determined.
  • The [Add angular dimension] dialogue box appears.

Notes

Even if you press Add Dimensions All , angular dimensions will not be added.
  • 3. Select the angular tolerance value you want to set from the pull-down menu.
  • If you do not have a desired tolerance, please specify it in the ‘Free input’ field.

Delete angular dimensions and angular tolerances

If you accidentally add dimensions or if dimensions are no longer needed, you can delete them.

Click Delete Settings , then click the dimension you want to delete.

Reselect the angle you want to display

If you want to change the viewing angle after the dimension is placed, you can choose again.

1. Click on Change below ‘Reselect angle’.

  • Once again, you will be able to select the position of the dimensions you want to display.

2.  Click the position of the angular dimension you want to set.

  • The display position of the dimensions is confirmed.
  • The tolerance values set before changing the viewing angle are carried over.

Recently viewed articles

    ↑