Measuring 3D models

To Measure Distance

Select the two points to measure, and the XYZ distance will be displayed in the window.
    1. Click
    2. Select the two points to measure.
 
    • (1)   Measurement icon
    • (2)   Selected object
    • (3)   Measurement window for each element
    • (4)   Switch measurement method window
    • (5)   Measurement component line

To Measure Diameter/Radius (R value)

Select the edge and face to measure, and the diameter/radius (R value) will be displayed in the window.
    1. Click
    2. Select the edge and face to measure.
 
    • (1)   Measurement icon
    • (2)   Selected object
    • (3)   Measurement window for each element (diameter/radius (R value))

To Measure Angle

Select the edge and face to measure, and the angle will be displayed in the window.
  1. Click
  2. Select the edge and face to measure.
 
    • (1)   Measurement icon
    • (2)   Selected object
    • (3)   Measurement window for each element (angle)

Screen introduction of measurement functions

Measurement icon

  • An icon used to measure various elements of the model
  • Shortcut key is activated by “Shift+M”.

Selected Objects

Various elements are displayed that can select the element need to measure

Tip

Sphere object Center point of the R edge
Cylindrical object Central axis of a curved surface

Measurement window by element

Window displaying information about the object to be measured and the numerical values of the decomposed XYZ components
Distance measurement R-value angle

Measurement mode switching window

Function to switch between longest and shortest distance measurements for selected elements
Longest distance Shortest distance

Measurement component line

Displays the XYZ components that configure the measured distance in mm

Tip

Black line Measurement result
Red line X direction component
Green line Y-direction component
Blue line Z direction component

Recently viewed articles

    ↑