The names of each tool and what you can do with these tools are specified below.
Function Name
What You Can Do
Reverse the Appearance
If the external appearance faces identified by meviy (faces colored in dark orange) are different from what you expected, you can invert the internal and external faces.
Add Dimensions
Add dimensions. → Adding Dimensions *It is not possible to add dimensions when the direction of measurement is at an angle.
Rotate the cube to change the orientation of the currently displayed parts.
Click [Isometric View] to return to the isometric view (default orientation),
(3) Display Settings
Move the mouse over the icon to display the display settings menu. Here you can change the 3D model display method, or toggle between displaying or hiding text information, weld location information and BOM table in the 3D viewer.
(4) PMI
PMI is an abbreviation of Product Manufacturing Information and refers to textual information for dimensions and holes. The position of the PMI display can be moved by dragging.