Difference in Shapes Between the 3D Model and the Finished Product

Points to Note on the Finished Shape of Internal and External Corners of Turning parts

Please check the examples and notes for differences in the finished product.
Models with sharp edges
Models with internal corners of less than C0.5/R0.5
Actual finished shape after machining

Tip

The finish conditions are as follows.
  • Models with external edges of less than C/R0.5 will have C/R 0.1 to 0.4 mm or slight chamfer.
  • If the internal corners of the cylinder are less than 0.5 and there is no relief groove in the model, the tool edge will leave a corner of R0-R0.4mm.
    →Click here to specify “Corner R0” without modeling a relief groove.

Caution

  • When modelled with ≥C0.5 mm or more, machining will be in accordance with the 3D data.
  • When modelled with ≥R0.5 mm or more, machining will be in accordance with the 3D data.

Caution

Specification of “no chamfer” is not supported.

Notes

Outer diameter grooving

Inner diameter grooving

Points to Note on Center Holes

The center hole made in the end face is used to keep the workpiece in place and to prevent core deviation when rotating the product.

Caution

  • 「”Center hole cannot be left” can be selected, but there may be restrictions on the shapes that can be machined that make the option unavailable. When this occurs, check the “Precaution” in the upper-left corner of the 3D Viewer.

Notes

(1) If you select “Remove center hole”, an arrow will point to the part.
(2) If the component has an inner diameter, no arrow will point to the part.

Points to Note on the Bottom of Holes (Machined and Cut)

A drill tip shape remains at the bottom of the hole (machined and cut).
Shape patterns Inner diameter hole does not have a step Inner diameter hole has a step
A
Drill tip shape remains (flat bottom will be 1mm or more)
B
Drill tip shape remains, no flat bottom
  • The type of the bottom of the hole will depend on the diameter and depth of the hole.
  • Example: If the inner diameter (D) is 10mm and the hole depth is 35mm, the depth of 35mm ÷ inner diameter of 10mm = 3.5D, so the bottom of the hole type will be B.
Inner diameter(D)the hole depth
 to 3D3D to 5D5D to 10D
D≦⌀6BBB
⌀6 <D≦⌀30ABB
⌀30<DAAA

If a flat bottom hole is required, please request it in “Additional Information”. We will confirm whether or not we can accommodate your request and reply.

Points to note regarding cylinder corners

Please check the examples and notes for differences in the finished product.

Outer diameter

①When “Corner R0 specification” is specified in the dialog
  • When you want to minimize the corner R or specify the relief groove
  • → Select “Corner R0”

Tip

Corner R0 has a width of less than corner R0.2 to R0.4, so the depth may be less than 0.5mm. You cannot choose.
① When machining with R0.4 tools
②When machining with R0.2 tools with R0.4 tools

③ If the length of the shaft is short, it may be machined with a tool with a 0.1mm radius on the end face that contacts the shaft.

Notes

In the following cases, “Corner R0” does not apply.
(1) The model has corner R0.5 or greater (2) The model has a relief groove
②If you specify “Corner R0 to R0.4 or less” in the dialog
  • When the cylindrical corner can be any shape
  • → Select “Corner Radius between R0 to R0.4”.

Tip

  • Arbitrary R shape of cylindrical corner
  • ① Machining R remains
  • ② Relief groove (1) Minimum clearance only at the cylindrical corner
  • Finished shape after

    Detailed figure

  • ③ Relief groove (2) Relief shape on cylindrical part + flange part
  • Finished shape after machining

    Detailed figure

③When modeling “corner R0.5 or more”
If the corners are modeled with R0.5 or higher, the shape will be as shown below.
  • Modeling of R0.5 or higher in corners
  • Finished shape after machining
  • Detailed figure

Inner diameter

Any relief groove below may be set.
  • Cross section
  • ①Detailed figure
  • ②Detailed figure

Notes

At the bottom left of the 3Dviewer, you can see the handling information for the cylindrical corners.

Points to Note on Incomplete Threads

The required undercut shape (length and depth) to ensure the threaded portion length for an incomplete threaded position is shown. See the example below.

[mm]

External Thread Internal Thread
Modelling Without undercut
With undercut
(1) Lower limit for the length of the incomplete thread and the width of the undercut. Pitch × 2.0 Pitch × 2.5 + 2
(2) Lower limit of the length of the threaded (external thread) and the depth of the threaded (internal thread). Pitch × 2.0 Pitch × 2.0
(3) Chamfered edge Chamfered to prevent burr Chamfered to prevent burr
(4) Minimum undercut depth value Pitch × 0.75 Pitch × 0.75

Caution

Parts with “Pitch × 0.75” or less set to the minimum value for the undercut depth(4) can be machined, but thread marks may occur.
  • Reference model
  • Actual finished shape after machining

Tip

  • The [Notes] shown in the red box below describe the applicable thread length/thread depth.
Example 1) Outer diameter specification: male thread thread length 44.6mm – 4.0 (pitch) x 2.0 = 36.6mm Example 2) Inner diameter specification: female screw thread depth 15.5mm – (1.0(pitch) × 2.5 + 2.0) = 11.0mm
内径情報指示

Caution

  • The thread shape cannot be identified. Set the outer and inner threads.
  • ねじ部は対象外形状として認識

Points to Note on the Tapered Thread (ISO)

  • Although there are multiple methods for modeling tapered pipe threads, the diameter and depth of the tapered pilot hole will be machined in accordance with ISO standards (or JIS B 0203). The modeled shape and depth of the hole are for reference only.
  • Other areas of the part that are not threaded, such as the area beyond the pilot hole, will be machined to the model.

Machined according to ISO standards (or JIS B 0203)

Machined according to the model

Points to note for the finished shape of the end-face groove inner corners

Check the examples and notes for differences from the final product.
Model with sharp edges in end face groove
Actual finished shape after machining
"*Finished with a radius (R) ranging from 0.1 to 0.5 mm. "

Notes

Since the shape is finished to R0.1 to 0.5, no modelling is required. Design with sharp edges.

Points to Note for the Finished Shape of Pocket Internal Corners

Check the examples and notes for differences from the final product.
Notch (pocket)
Shape of less than R0.5 including sharp edges
Actual finished shape after machining
"*Finished with a radius (R) ranging from 0.1 to 0.5 mm. "

Caution

  • The machined curve on the sides of the pocket depends on the tool diameter, which is chosen as small as possible.
  • If there are any discrepancies between the model and the finished form, please feel free to let us know.
  • ねじ部は対象外形状として認識

Points to Note for Sliting processing

The dimensions of the parts may change as a result of the slitting process. Therefore, the dimensions of the following shapes are guaranteed based on the measurements taken before slitting.

Hexagonal Hole Notes

Information and examples of differences between the model and the finished part.

  • The shape of the finished hexagonal hole will vary depending on the distance across the flats.
  • The modeled depth is used as a reference, and the shape of the bottom of the hole will vary.

Hexagonal Hole corresponding shapes and sizes

Distance across the flats Metal Resin
2 Finished Shape①
2.5
3
4
5
6 Finished Shape②
8

Caution

The roughness specified for the surface does not apply to the internal hexagon.

Finished Shape①

Distance across the flatsMetalResin
OtherFinished Shape②

Notes

The tolerance for the distance across the flats meets to the JIS B 1176.

Finished Shape②

Recently viewed articles