- HELP
- How to use
- Before You Begin
- Automatic hole / inner diameter type Recognition
- Automatic Recognition of hole / inner diameter type from Color Attributes
Automatic Recognition of hole / inner diameter type from Color Attributes
The colour displayed on the side of the hole in the model is automatically recognised, and the hole and inner diameter type can be reflected in meviy by matching it with the pre-registered value.
Setup Method
STEP1:
STEP2:
Select “SOLIDWORKS”, “iCAD”, or “CATIA” from the CAD in use drop-down list.
STEP3:
To recognize the hole/inner diameter type: select “Automatic recognition of hole/inner diameter type from color attributes” from the drop-down menu.
STEP4:
Check the ON/OFF button for the hole/inner diameter type you want to set and activate the RGB entry field.
Put the values in RGB.
Note: RGB should be set at a value of 0~255.
| Items | Details | |
|---|---|---|
| 1 | ON/OFF | It is possible to switch the setting on and off for each hole/inner diameter type. |
| 2 | Hole/Inner Diameter type | This is a list of hole/inner diameter types that can be automatically recognized by color attribute linking. |
| 3 | RGB | This field is used to register the color attributes, with a value between 0 and 255 for each RGB. |
| 4 | Colour check | A message about the status of the RGB settings is displayed. |
STEP5:
You can specify how the hole type is recognized when the color attributes (RGB values) do not match.
Select one of the following options from the drop-down menu:
①Automatic recognition of tapped holes from hole diameter
If the color attribute is not linked, the threaded hole is automatically recognized based on the hole diameter.
Automatic recognition of tapped holes from hole diameter
②All through holes, straight holes, recognized without tolerance
If the color attributes are not linked, it is recognized as a straight hole or a through hole.
Click “Save Settings” at the bottom of the page.
After uploading the data:
(1) Hover the mouse over [ Menu
] in the 3D viewer.
(2) Click [ Display automatic hole recognition results and colour attributes
].
(3) The list of holes in the details displays information about the linked color attributes.
(4) To recognize the hole and inner diameter type: select “Automatically recognize threaded holes based on hole diameter (without inner diameter)” from the drop-down menu.
Tip
- There are limitations to the CAD data that can be linked to colour attributes.Please refer to the table below, ‘3D CAD format for colour attributes‘.
Caution
Restrictions apply to the types of hole and inner diameter that can be linked from the colour attribute.Please refer to the following precautions and adjust the meviy settings as required.
-
The effective depth of each hole is independent and reflects the user’s settings.
Set the effective depth for each item using the following user settings. - Quotation Settings for Machined Plates Tapped Holes
- Quotation Settings for Turning Parts Tapped Holes
- Quotation Settings for Machined Plates Precision Holes
- Quotation Settings for Turning Parts Precision Holes
- Tapped holes/Internal threads will not be linked to meviy unless the pilot hole diameter and specified colour (RGB) match for each CAD system.
- Please refer to the following for the pilot hole diameters for each CAD system.
- → CNC Milling > Recognizing Different Types of Hole
- → CNC Turning > Specifications for External Thread and Internal Thread, Keyways, Holes and Pockets
- → Sheet Metal Parts > Tapped Hole Identification and Selectable Sizes
-
This function does not link the machining direction.If the pilot hole is penetrated, check the machining direction.
・3D CAD format for colour attributes
| CAD softwares | Native | Intermediate format(Parasolid) | ||
|---|---|---|---|---|
| (.sldprt)(.icd)(.CATPart) | .x_t | .x_b | .xmt_txt | |
| SOLIDWORKS |
〇 |
〇 |
〇 |
– |
| iCAD SX |
〇 |
〇 |
〇 |
〇 |
| CATIA |
〇 |
– |
– |
– |
Caution
The automatic recognition of hole/inner diameter type from color attribute is not guaranteed for models created with non-compatible CAD systems or formats.